Here's one for someone who knows the SigmaDSP internals (Dave, is this one for you ?)
Our products make use of the S/PDIF input on the ADAU1452 and ADAU1467, usually through one of the ASRC blocks - but we have had a customer who has asked if we can do it without the ASRC !!
We have explained that the Sending Device would have to be locked to the same Sample Rate clock (in our case this would be a Dante Network Audio system) and they are OK with that.
My question is - While specifying that the ASRC is driven by the SPDIF and taken a signal from the ASRC block, is there a way to take a signal directly from the SPDIF input into the Schematic and then use a switch to select one or the other ?
EDIT: I should add that I found in the ADAU1467 data-sheet (page 50) that it says "The S/PDIF receiver can be accessed directly in the DSP core by using the S/PDIF input cell" - but I can't find the S/PDIF Input Cell in the Toolbox Tree in Sigma Studio.
Thanks
PhilipJ
Edit Notes
added an Edit note at the end[edited by: philipj451 at 1:23 PM (GMT -4) on 16 Jul 2026]