Post Go back to editing

ADAU1466:How can I retrigger GainEnvelope on every guitar pick attack?

Thread Summary

The user is working on an ADAU1466 SigmaStudio project to create a banjo-like decay for a hexaphonic guitar. The issue is that the GainEnvelope block does not retrigger on subsequent pick attacks while the string is still ringing. The solution involves using a Peak Envelope block, a Hamming differentiator, a comparator, and a OneShot to detect new attacks and retrigger the envelope. Adjusting the Peak Envelope hold time, comparator threshold, and OneShot duration helps mitigate false retriggers and ensures reliable attack detection, even with natural string amplitude fluctuations.
AI Generated Content
Category: Software
Software Version: SigmaStudio 4.7

Hello,

I am working on an ADAU1466 SigmaStudio project for a hexaphonic guitar.

My goal is to create a banjo-like decay characteristic, where the note decays much faster than a normal guitar while preserving the natural attack.

I am using a GainEnvelope block, but I have a problem:

The GainEnvelope starts correctly on the first pick attack. However, once triggered, it always completes its programmed cycle and cannot be retriggered by a new pick attack while the string is still ringing.
For example:

Pick a string
Let it decay to approximately -20 dB
Pick the same string again

Ideally, the second pick attack should restart the GainEnvelope from the beginning. Instead, the new note is affected by the remaining state of the previous envelope cycle, causing the second note to sound quieter than intended.

My question is:

What is the recommended SigmaStudio method for detecting every new guitar pick attack, including attacks that occur while the previous note is still sounding?

This is especially important for fast playing, where multiple notes may be picked before the previous note has fully decayed. The final goal is not note-on detection from silence, but reliable attack detection on an already ringing guitar string.

Is there a dedicated SigmaStudio block for this purpose, or is a custom transient/attack detector the recommended approach?

The platform is ADAU1466 running in SigmaStudio without an external MCU.

Any ADAU1466 / SigmaStudio specific suggestions would be greatly appreciated.

Thank you.

Thread Notes

Parents
  •      Hello,

         The issue you found reminds me of a '50s (?) song, Johnny B. Goode -- he could "play a guitar just like ringing a bell."  Bells are known for rhythmic waves of harmonics with varying amplitudes and phases.  To synthesize a bell sound you needed balanced modulators, which weren't cheap back in the 70s.   In the DSP world, a multiplier does it.  DSPs are multiply-and-add machines, so the chip you're working with has literally thousands of them!   I grew up with vacuum tubes, so what little I know about DSP is from reading a few books and playing with SigmaStudio.  You'll have fun doing the same.

         It's no surprise that a real-world input would cause issues, although I didn't expect this one.   I added modulation to my simulated "guitar" although having no idea of how much modulation (or, "ripple") in the guitar signal would be present:

    Then I made the incoming signal increasingly "difficult" for the project to handle until it just couldn't.  In the scope traces that follow, the top trace is the output at PeakEnv1, the bottom is the project's audio output.

         This first example is with no modulation and a strum rate of 10 Hz.  The stairstep in the decay is from the 10mS "hold" setting of PeakEnv1.  We set this to reject ripple from individual cycles of the input waveform -- thus we need more hold when lower audio frequencies are present.  Ten mS is enough to cover a 50 Hz input, which has a period of 20 mS and thus a time of 10 mS between peaks (all SigmaStudio level detectors are full-wave; in DSP this is merely "absolute value").  You can make this shorter if 50 Hz is never present, or longer for a holdoff against multiple triggering, as you have suggested.

         This one is with 5 Hz, -10dB (roughly 30%) modulation, with a low 1 Hz strum rate.  It works fine here.

         It gets difficult when the modulation rate and the strum rate are nearly equal -- here, 10 Hz and 8 Hz respectively.  Also the modulation has been increased to -6 dB (50%).  The project cannot make sense of this chaos.  It appears that banjo picking is often even faster, so it mayl be tough to separate the modulation from the picking.

         Presently, I don't know exactly how to fix this, yet it's something we can work on together.  You said your DSP experience is limited, but if you have analog EE experience this is quite helpful.  SigmaStudio is great for building analog-like circuits and you won't burn your fingers on a soldering iron!   There’s a few guitar enthusiasts on EZ who might jump in and help.

         Edit:  By the way, you can retrigger the Envelope block by interrupting its control input (that is, setting it to zero) for just one sample interval.  Yet, presently this isn't useful since we're having trouble with the basic idea.

         Best regards,

         Bob

  • Hi Bob,

    I finally had some time to really dig into the project. Based on what I've learned while working with it, I honestly think your solution works extremely well! Blush

    It actually didn't take very long to get the basic idea working. After just a few hours I found that most of the retriggering problems could be eliminated by carefully adjusting a few parameters. My guess is that the random retriggers were caused by the uneven decay of a real guitar string. During the decay, the system occasionally interpreted changes in the envelope as a new attack, so the note would suddenly jump back to full volume.

    The two settings that helped the most were the ZeroComp bit value and the OneShotRise timer. After that I fine-tuned the Peak Envelope Hold and Gain values.

    Once I had eliminated the retriggers, I noticed another issue: sometimes very soft picking wouldn't trigger the effect. I also found that after a loud pick, a softer but still intentional pick—or even several in a row—would sometimes fail to retrigger. Instead, the string would continue playing at whatever reduced level the Slew Volume was currently producing. So I kept experimenting with the Hold and Gain settings until I found a combination that solved both problems.

    After that I tried every playing dynamic I could think of, from the lightest touch to very aggressive picking, and the trigger became completely reliable without unwanted retriggers. It even responds to the slightest touch on the string, not just normal picking.

    It took me about one full day to optimize a single string for every possible playing situation, then another day to repeat the process for all six strings. (For me that's about 14 hours... if I start something, I tend to do it properly. Smile)

    Then I made a "mistake" during testing. While working on one string, I had disabled the pickups for the other strings. Everything looked perfect. But when I turned all the pickups back on and started playing chords, I suddenly got frequent retriggers again. It turned out that each pickup, although much quieter, still picks up the neighboring strings.

    In the end I'm actually glad this happened because it showed that the main limitation wasn't your algorithm—it was pickup crosstalk.

    The behavior makes sense. Different notes decay differently, both in level and over time, and occasionally the algorithm interprets those changes as a new attack. So I had to go back and adjust everything again. That took about another week, but eventually I managed to get the dynamic behavior working exactly the way I wanted on all six strings.

    My priority was making sure every intentional pick would always trigger. I do still get the occasional retrigger, but only after a chord has almost completely decayed (with the fast banjo-style decay), when the strings are already extremely quiet. In practice this really isn't a problem. It's a fairly uncommon playing situation, and the retriggered notes are so quiet that they're hardly noticeable. In fact, accidental string noises during normal playing are usually more obvious than these occasional retriggers—and even professional players produce those kinds of noises.

    One interesting thing I noticed at the end: throughout my testing I kept the Slew Volume release (decay) time fixed and eventually became curious about how short I could make it. As I reduced the decay time, the old problems gradually started coming back. Below a certain minimum value—which was slightly different for each string—soft picks stopped triggering reliably again, and harder picks sometimes produced immediate retriggers. I could improve things somewhat by fine-tuning the other parameters again, but eventually I reached a practical limit below which I couldn't shorten the decay any further. That's perfectly fine though, because I don't actually need it any shorter.

    So in the end, getting the system to work well with chords required only a very small compromise. It might even be possible to optimize it a little further, but from a practical playing perspective I'm completely satisfied with it now.

    The system really works. And if I decide to redesign my pickups in the future to reduce crosstalk, I think the results could be even better, because at the beginning—before crosstalk became part of the picture—I wasn't seeing these problems at all.

    I've attached a WAV recording as well. For this recording I intentionally set the release (decay) time a little shorter than what I'd normally use, just to push the system a bit. Even with this setting, false retriggers are still very rare.

    Thanks again for all your help! I really appreciate the time you spent putting this project together.

Reply
  • Hi Bob,

    I finally had some time to really dig into the project. Based on what I've learned while working with it, I honestly think your solution works extremely well! Blush

    It actually didn't take very long to get the basic idea working. After just a few hours I found that most of the retriggering problems could be eliminated by carefully adjusting a few parameters. My guess is that the random retriggers were caused by the uneven decay of a real guitar string. During the decay, the system occasionally interpreted changes in the envelope as a new attack, so the note would suddenly jump back to full volume.

    The two settings that helped the most were the ZeroComp bit value and the OneShotRise timer. After that I fine-tuned the Peak Envelope Hold and Gain values.

    Once I had eliminated the retriggers, I noticed another issue: sometimes very soft picking wouldn't trigger the effect. I also found that after a loud pick, a softer but still intentional pick—or even several in a row—would sometimes fail to retrigger. Instead, the string would continue playing at whatever reduced level the Slew Volume was currently producing. So I kept experimenting with the Hold and Gain settings until I found a combination that solved both problems.

    After that I tried every playing dynamic I could think of, from the lightest touch to very aggressive picking, and the trigger became completely reliable without unwanted retriggers. It even responds to the slightest touch on the string, not just normal picking.

    It took me about one full day to optimize a single string for every possible playing situation, then another day to repeat the process for all six strings. (For me that's about 14 hours... if I start something, I tend to do it properly. Smile)

    Then I made a "mistake" during testing. While working on one string, I had disabled the pickups for the other strings. Everything looked perfect. But when I turned all the pickups back on and started playing chords, I suddenly got frequent retriggers again. It turned out that each pickup, although much quieter, still picks up the neighboring strings.

    In the end I'm actually glad this happened because it showed that the main limitation wasn't your algorithm—it was pickup crosstalk.

    The behavior makes sense. Different notes decay differently, both in level and over time, and occasionally the algorithm interprets those changes as a new attack. So I had to go back and adjust everything again. That took about another week, but eventually I managed to get the dynamic behavior working exactly the way I wanted on all six strings.

    My priority was making sure every intentional pick would always trigger. I do still get the occasional retrigger, but only after a chord has almost completely decayed (with the fast banjo-style decay), when the strings are already extremely quiet. In practice this really isn't a problem. It's a fairly uncommon playing situation, and the retriggered notes are so quiet that they're hardly noticeable. In fact, accidental string noises during normal playing are usually more obvious than these occasional retriggers—and even professional players produce those kinds of noises.

    One interesting thing I noticed at the end: throughout my testing I kept the Slew Volume release (decay) time fixed and eventually became curious about how short I could make it. As I reduced the decay time, the old problems gradually started coming back. Below a certain minimum value—which was slightly different for each string—soft picks stopped triggering reliably again, and harder picks sometimes produced immediate retriggers. I could improve things somewhat by fine-tuning the other parameters again, but eventually I reached a practical limit below which I couldn't shorten the decay any further. That's perfectly fine though, because I don't actually need it any shorter.

    So in the end, getting the system to work well with chords required only a very small compromise. It might even be possible to optimize it a little further, but from a practical playing perspective I'm completely satisfied with it now.

    The system really works. And if I decide to redesign my pickups in the future to reduce crosstalk, I think the results could be even better, because at the beginning—before crosstalk became part of the picture—I wasn't seeing these problems at all.

    I've attached a WAV recording as well. For this recording I intentionally set the release (decay) time a little shorter than what I'd normally use, just to push the system a bit. Even with this setting, false retriggers are still very rare.

    Thanks again for all your help! I really appreciate the time you spent putting this project together.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.