Post Go back to editing

ADAU14xx dejitter performance, and MCLK requirements

Thread Summary

The user inquires about the dejitter performance of the ADAU1452 and ADAU1463, specifically the range of jitter correction on MCLK input, the impact on CLKOUT jitter, and the jitter range for serial port clocks. The support engineer explains that dejitter is primarily managed through buffers and clock period synchronization, and mentions that the core start bit, often derived from an internal source post-PLL, helps reduce jitter. The engineer will look for more detailed test data and suggests a meeting to discuss further.
AI Generated Content
Category: Hardware
Product Number: ADAU1463

The ADAU1452 and ADAU1463 data sheets mention automatic dejitter for the clock generator, and also specify that CLKOUT has anywhere from 12 ps to 206 ps of jitter.

I am curious about the performance of the dejitter function, and where it is effective.

A) How much can the dejitter correct? Is there a range of allowed jitter on the MCLK input that can be corrected? ... or is there a limit to the dejitter performance?

B) It appears from the diagrams that dejitter is certainly applied to the clock generators for the serial ports, but it's unclear whether dejitter also improves the CLKOUT quality.

i.e. Is CLKOUT jitter of 12 to 206 ps guaranteed no matter what jitter MCLK has?

C) Assuming dejitter is automatic for all serial port clocks, what is the jitter range there? (I am assuming it may be different from the provided specifications for CLKOUT)

I have designed a board with the ADAU1463 and two AD2437 chips, with the ability to switch MCLK on the SigmaDSP from either a low-jitter oscillator or the CLKOUT2 signal from the primary A2B chip. I'm curious how much the low-jitter oscillator actually helps when the ADAU1463 is master, and how much worse the jitter might be when taking the CLKOUT2 from A2B to MCLK.

Thread Notes

  • Hello SoundConsulting,

    Gee, this part was designed over ten years ago and I am not sure what information we might have for actual measured data. I will look around.

    A lot of the dejitter is done by using buffers. The serial ports are help for one clock period. This also allows for managing LRCLK inputs that might be slightly delays one to the other from two different parts that are running on the same MCLK but the LRCLK edge is slightly skewed. 

    So after a sample period. the serial port data is transferred to some holding memory until the next sample period starts. 

    The sample period for the core is set by the core start bit. That is often from an internal source which is after the PLL so less jitter. 

    I will look to see what info I might find from the original testing but we should have a meeting and discuss. 

    Thanks,

    Dave T

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.