Post Go back to editing

R-theta-JA (Junction to ambient thermal resistance) for ADSP-21565BSWZ8

Category: Datasheet/Specs
Product Number: ADSP-21565BSWZ8

Hi Greetings!!

We are using 'ADSP-21565BSWZ8' part in our upcoming design.

We would like to perform thermal analysis and simulation.

Could you please provide 'R-theta-JA (Junction to ambient thermal resistance)' for ADSP-21565BSWZ8 part?

Thank you in advance,

Mihir

Parents
  • Hi Mihir,

    Please refer ENVIRONMENTAL CONDITIONS"(Page No: 88/102)  in the ADSP-21565 datasheet linked below:
    www.analog.com/.../adsp-21562-21563-21565-21566-21567-21569.pdf

    Regards,
    Divya.P

  • Hi,

    I am also looking for below parameters:

    1. R-theta-JC (Junction to top Case thermal resistance)

    2. R-theta-JB (Junction to Board thermal resistance) / R-theta-JC (bot) (Junction to bottom Case thermal resistance)

    Kindly provide the above mentioned data as early as possible.

    Regards,

    Mihir

  • Hi Mihir,

     Apologies for the delay.


    As mentioned earlier, the use of JEDEC qJA, qJC, or YJT thermal parameters for application system thermal estimates is not recommended as indicated in the JEDEC51 specifications.

    Regards,
    Divya.P

  • The thermal simulation is not feasible (or even possible) when selecting components, and with R-theta-JA value we (your customers) could make a ROUGH estimate, even it is not recommended.

    Modeling a PCB without actually making the PCB is really difficult. I used (tried at least) flotherm and depending on the model i got junction temperatures of 120 to 300 C.

    Also, in your model the exposed pad is higher than the LQFP leads so there will be airgap when using high resolution grid.

    So please can you provide here the RJA (and others) value for LQFP and BGA packages?

    With this value, it makes easier to get started with at least some confidence to Your product, that it does not smoke in our environment. There is a good excel to make the power estimate on different clock frequencies. We run the simulations when we have constructed the PCB layout and surrounding mechanics.

Reply
  • The thermal simulation is not feasible (or even possible) when selecting components, and with R-theta-JA value we (your customers) could make a ROUGH estimate, even it is not recommended.

    Modeling a PCB without actually making the PCB is really difficult. I used (tried at least) flotherm and depending on the model i got junction temperatures of 120 to 300 C.

    Also, in your model the exposed pad is higher than the LQFP leads so there will be airgap when using high resolution grid.

    So please can you provide here the RJA (and others) value for LQFP and BGA packages?

    With this value, it makes easier to get started with at least some confidence to Your product, that it does not smoke in our environment. There is a good excel to make the power estimate on different clock frequencies. We run the simulations when we have constructed the PCB layout and surrounding mechanics.

Children