Post Go back to editing

I am not able to set the PLL CTL and PLL DIV Register- ADSP BF548 custom board.

Category: Software
Product Number: : ADSP-BF548, silicon 0.4
Software Version: visual dsp++5.1.2.0

i am current working on ADSP BF548 custom board, I am able to set the PLL CTL and PLL DIV Register. However, I am unable to check the SCLK values in my code; is there a way to do so? I've attached my code for reference.
Please assist me since I too want to write code for the spi protocol.


ADI_SYSCTRL_VALUES sys_cntrl_write;
ADI_SYSCTRL_VALUES sys_cntrl_read;

// Set CCLK = 400 MHz, SCLK = 133 MHz, voltage to 1.25v
sys_cntrl_write.uwPllCtl = 0x2000;
sys_cntrl_write.uwPllDiv = 0x0003;
sys_cntrl_write.uwVrCtl = 0x40EB;

bfrom_SysControl ( SYSCTRL_READ | SYSCTRL_PLLCTL | SYSCTRL_PLLDIV |
SYSCTRL_VRCTL | SYSCTRL_INTVOLTAGE, &sys_cntrl_read, NULL );

printf("Before Set PLLCLT Reg : 0X%X\n",sys_cntrl_read.uwPllCtl);
printf("Before Set PLLDIV Reg : 0X%X\n",sys_cntrl_read.uwPllDiv);
printf("Before Set VRCTL Reg : 0X%X\n",sys_cntrl_read.uwVrCtl);

bfrom_SysControl( SYSCTRL_WRITE | SYSCTRL_PLLCTL | SYSCTRL_PLLDIV |
SYSCTRL_VRCTL | SYSCTRL_INTVOLTAGE, &sys_cntrl_write, NULL);

bfrom_SysControl ( SYSCTRL_READ | SYSCTRL_PLLCTL | SYSCTRL_PLLDIV |
SYSCTRL_VRCTL | SYSCTRL_INTVOLTAGE, &sys_cntrl_read, NULL );

printf("After Set PLLCLT Reg : 0X%X\n",sys_cntrl_read.uwPllCtl);
printf("After Set PLLDIV Reg : 0X%X\n",sys_cntrl_read.uwPllDiv);
printf("After Set VRCTL Reg : 0X%X\n",sys_cntrl_read.uwVrCtl);

results from the board : 

  • ADI North America will be on annual shutdown December 24, 2022 through January 2, 2023; perhaps another community member can assist you until our return on January 3.
  • Hi,

    User-programmable value divides the VCO signal to generate the system clock (SCLK). You can calculate SCLK by using below formula SCLK = VCO/PLL_DIV.SSEL

    VCO is calculated by VCO = (SYS_CLKIN frequency/(DF+1)) MSEL. Please refer " 18 DYNAMIC POWER MANAGEMENT " in below linked HRM:www.analog.com/.../ADSP-BF54x_hwr_rev1.2.pdf

    Attached SPI transmission and reception example for BF592 across 2 EZkits. You can refer this for BF548.
    SPI_ADSP-BF592.zip
    Regards,
    Divya,P

  • #include <sys/platform.h>
    #include "adi_initialize.h"
    #include "PSRDev.h"
    #include<stdio.h>
    #include "../lib/src/drivers/source/spi/adi_spi_data_bf5xx.c"
    
    #include <services/pwr/adi_pwr.h>
    #include <sys/platform.h>
    #include <drivers/spi/adi_spi.h>
    #include <../include/services/pwr/adi_pwr_bf5xx.h>
    #include <bfrom.h>
    #include <blackfin.h>
    #include <stdio.h>
    #include <drivers\uart\adi_uart.h>
    #include <services\pwr\adi_pwr.h>
    
    
    int main()
    {
    	
    		uint32_t clkIn 		= 25 * 1000000;
    		uint32_t coreMax	= 400 * 1000000;
    		uint32_t sysclkMax	= 100 * 1000000;
    		uint32_t vcoMin		= 50 * 1000000;
    
    		ADI_PWR_VOLTAGE adiPwrV_default,adiPwrV_User;
    		uint32_t fSclk,fCclk;
    
    
    		if(adi_pwr_Init(clkIn, coreMax, sysclkMax, vcoMin) != ADI_PWR_SUCCESS)
    		{
    			REPORT_ERROR("Failed to initialize power service \n");
    			return FAILED;
    		}
    
    			if(adi_pwr_SetInternalVoltage(ADI_PWR_VOLTAGE_125,coreMax,sysclkMax) != ADI_PWR_SUCCESS)
    		{
    			REPORT_ERROR("Failed to Set Internal Voltage \n");
    			return FAILED;
    		}
    
    		if(adi_pwr_GetInternalVoltage(&adiPwrV_User))
    		{
    			REPORT_ERROR("Failed to Get Internal Voltage \n");
    			return FAILED;
    		}
    
    		printf("USER SET ...ADI PWR Voltage = %d \n",adiPwrV_User);
    
    		if(adi_pwr_GetSystemFreq(&fSclk) != ADI_PWR_SUCCESS)
    		{
    			REPORT_ERROR("Failed to Get System Freq \n");
    			return FAILED;
    		}
    
    		if(adi_pwr_GetCoreFreq(&fCclk) != ADI_PWR_SUCCESS)
    		{
    			REPORT_ERROR("Failed to Get core Freq \n");
    			return FAILED;
    		}
    
    		printf("SET... FSCLK = %d \t SET...FCCLK = %d\n",fSclk,fCclk);
    
    		(*pPORTB_FER) = (*pPORTB_FER) | 1<<9; // chip select 1
    		*pPORTB_FER = (*pPORTB_FER) | 1<<12; // SPIXSCK 1
    		*pPORTB_FER = (*pPORTB_FER) | 1<<13; // SPIXMOSI  1
    		*pPORTB_FER = (*pPORTB_FER) | 1<<14; // SPIXMISO  1
    
    		ssync();
    
    		*pSPI2_CTL	=	0x4600;///
    		*pSPI2_FLG  = 0x0002;  //FLS1 (SPI2 Slave Select 1);
    		*pSPI2_BAUD = 24;
    		ssync();
    
    		//open the SPI driver
    		result = adi_spi_Open(2, driverMemory,ADI_SPI_DMA_MEMORY_SIZE, &hSPI2Device);
    		printf("adi_spi_Open result = %d \n",result);
    
    		while(1);
    }


    /* Device name = ADSPBF-548
    Hello, I'm setting a serial clock for an SPI2 device using the code below.
    If anyone could help, it would be greatly appreciated. Tell me what I'm doing incorrectly and why a decent serial clock isn't being generated.
    Can someone kindly offer some advice on the steps I should take to put the SPI2 device up as a slave so that it produces the 25 MHz serial clock I need?
    */                                                                                                                                                                                                                                                                                                               



    /*------- OUTPUT WHICH IM GETTING FROM THIS CODE------*/
    Load complete.
    Default...ADI PWR Voltage = 15
    Default...FSCLK = 50000000 Default...FCCLK = 200000000
    USER SET ...ADI PWR Voltage = 14
    SET... FSCLK = 100000000 SET...FCCLK = 400000000
    adi_spi_Open result = 0 

  • Following your advice, I am now able to set the PLL registers. I have configured the board with the standard UART protocol which works as expected.
    Thank you for your help...

    Now I need to configure the PORTB register pins (PB9, PB12, PB13, PB14) as GPIO output pins and I want to see the high/low control of these pins, but the code I have provided below has no outputs. This code is based on the ADSPBF-548 datasheet.


    *pPORTB = PB9 | PB12 |PB13 | PB14; // GPIO Pin high

    (*pPORTB_FER) = (*pPORTB_FER) & ~(1<<9); 
    (*pPORTB_FER) = (*pPORTB_FER) & ~(1<<12); 
    (*pPORTB_FER) = (*pPORTB_FER) & ~(1<<13);
    (*pPORTB_FER) = (*pPORTB_FER) & ~(1<<14); 

    *pPORTB_FER = PB12 | PB13 | PB14;//Enable pins
    ssync();

    (*pPORTB_MUX) = (*pPORTB_MUX) & ~(1<<18); // chip select 1
    (*pPORTB_MUX) = (*pPORTB_MUX) & ~(1<<19); // chip select 1


    My request is please help me too figure it out, how to configure these pins as GPIO or tell me what I am doing wrong to configure it.
    If you have any articles or examples on this please let me know.

  • Hi ,

    Please download ADSP-BF548 EZ KIT Board Support Package (Rev. 1.0.0)  from the below link:
    download.analog.com/.../ADI_ADSP-BF548_EZKIT-Rel1.0.0.exe

    After installation examples available in the below path:
    <Installation path>\ADSP-BF548_EZKIT-Rel1.0.0\BF548_EZ-Kit_Lite\Blackfin\Examples

    Refer Button_LED_GPIO example for GPIO output.

    Also, refer "Programming Model" in the below linked HRM for more details about GPIO
    www.analog.com/.../ADSP-BF54x_hwr_rev1.2.pdf

    Regards,
    Divya.P

  • hi,

    we are not able to download this download.analog.com/.../ADI_ADSP-BF548_EZKIT-Rel1.0.0.exe software.

    is there any other way ,so ,we can download this example..    

  • Hi,

    We have attached GPIO example. Please refer the same.  Regarding BSP download, please try with different browser.Button_LED_GPIO.zip

    Regards,
    Divya.P

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.