I would like to use two noise reduction circuits for the ADI algorithm on the ADAU1452.
When I compiled it, it was impossible due to insufficient DataMemory capacity.
When I checked only the noise reduction 1 circuit of the sample, more than half of the capacity of "DM0" was used.
If we can specify some blocks for "DM1", we think that it is possible to use two systems.
Is there a way to specify "DM1" and place the circuit?