Post Go back to editing

BF706 ECC Resets

Hi Forum

I have an application that runs fine in the field. 

However rarely the board resets, due to watchdog reset, but I have yet to see in in LAB.

As my program uses the L2 memory, for both program and data, I am wondering if it could be an error in the L2 memory that causes the reset. I have not disabed the ECC, for any part of the L2 memory.

If I read the manual it states:

___________________

An ECC multi-bit error in an ECC-enabled bank. A non-modulo, 32-bit write to an ECC-enabled bank can
also potentially create a bus error response due to an ECC multi-bit error. This response is because the L2 system
memory implements a 32-bit ECC, and therefore a non-modulo, 32-bit write results in a read. This read
can create multi-bit errors even if the memory was initialized.

___________________

Could this cause a reset? And would it help to disable the ECC for the data part?

Alternatively I also read from the manual:

___________________

If data in L2 SRAM contains single-bit errors, the data is corrected on its way to the system buses. The corrected
value is not written back to the SRAM location. To prevent any risk of accumulation of single-bit errors over time
and to minimize likelihood of multi-bit errors, the L2 system memory provides a special memory refresh mechanism.

___________________

Could this be the cause, that errors are build up? How likely is that, and should I enable SCRUB.. and how does it work?

  • Hi,

    Error correcting codes (ECC) are used to correct single event upsets. The L2 memory is protected with a single error correct-double error detect (SEC-DED) code. By default ECC is enabled, but it can be disabled on a per-bank basis.

    1. Please try the application after disabling ECC.
    2. Please check whether you are installed the  INTR_L2CTL0_ECC_ERR interrupt in adi_int_InstallHandler.

    Regards,
    Anand Selvaraj.