Hello
I tried this example given in the forum for SC584 EZ kit.
[FAQ] Example project which helps to understand how to interface flash SPI using driver APIs
The program runs fine and it displays on console the flash basic information. I ran this project in debug mode when my Switch SW1 is in position 1 which is actually Boot from Flash Mode. After running this project and again powering off and then on the board the system fault red LED is glowing continuously. And when I try to flash the chip in no boot mode and again resetting the board after changing the SW1 position to 1 then also led still continuously glows and my project didn't boot from the flash. This same behavior happen on two of my evaluation kit and in both now I am not able to boot my project from flash. What might be the issue can you guide me? It will be of great help.
Regards
Anukul Anand