Post Go back to editing

ADSP-BF51x L1 allocations

Tools: CCES 2.2.0, ADSP-BF518F EZBOARD
On the ADSP- B51x can an L1 data bank(ex. B) be allocated for instruction or can an instruction bank be allocated for data? Perhaps a modification to the LDF file?

If so, what are the ramifications?

Is there bus contention?

Can all(except scratch) of L1 be allocated to either code exclusively of data exclusively? This assumes there is an external allocation for the other one.

  • Thanks,

    I was not sure since the datasheet says the following:

    "Blackfin processors support a modified Harvard architecture in

    combination with a hierarchical memory structure. Level 1 (L1)

    memories are those that typicallyoperate at the full processor

    speed with little or no latency. At the L1 level, the instruction

    memory holds instructions only. The two data memories hold

    data, and a dedicated scratchpad data memory stores stack and

    local variable information." pg4

    ADSP-BF512_514_514F16_516_518_518F16

    Additionally in the ref. the Chip Bus hierarchy diagrams show data buses between the L1 and Processor core and showing data and instruction separately in multiple figures. I understand figures can often require clarification.

    ADSP-BF51x Blackfin Processor Hardware Reference

    I was able to re-assign Data Bank B cache(FF904000 - FF907FFF) and place some lib_code there.

    Thanks,

    Nathaniel

  • After more testing I received an access violation when I tried to access code from the 0xFF90 000 memory region aka Data Bank B.

    It appears I am able to store code there, but the proc. still thinks the region is for data. This means that trying to access the code results in a fault unless there is way to tell the proc. that its code.

    A non-recoverable error or exception has occurred.

      Description:   Illegal instruction fetch access (memory protection violation) (Exception with EXCAUSE=0x2B).

      General Type:  UnhandledException

      Specific Type: InstructionFetchViolation

      Error PC:      0xff900000

    Thanks,

  • Hi,

    Apologies for any confusion

    Please note that Blackfin L1 data memory can't be used for instructions and L1 instruction memory can't be used for data.

    Please let me know if you need further details

    Best Regards,

    Kader

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.