All,
I have two development boards ADZS-SC584-EZLITE. And I want to establish connection between them via SPORT. The purpose is to communicate between two DSP's. What all I need and how to do this in a simple way?
Thanks!
All,
I have two development boards ADZS-SC584-EZLITE. And I want to establish connection between them via SPORT. The purpose is to communicate between two DSP's. What all I need and how to do this in a simple way?
Thanks!
Hi,
Please refer the below which explains how to validate SPORT on ADSP-SC58x processors. The below link contains the SPORT example code, please use the code as a reference and modify as per your requirement. You can understand the working of the code from the comments embedded within.
ez.analog.com/.../how-do-i-validate-the-sport-on-my-newly-designed-board-based-on-adsp-sc58x-adsp-2158x-processors
Regards,
Anand Selvaraj.
Hi,
I found that the expansion slot Expansion Interface III Connectors (P1A-C) is used for SPI, TWI, UART, SPORT, and GPIO interfaces of the processor. FX8-120S-SV(21) is the mating connector to be used. Using that we can establish connection between two development boards. Is there any standard ready made cable/connectors available to buy?
Thanks.
Hi,
Apologies for the delay.
Unfortunately, there is no standard ready made cable/connectors available. You can customize the cable/connectors as per the requirement.
Regards,
Anand Selvaraj.