ADSP 21060 and ICE2000 emulator

We have to debug and reprogram some 21060 based equipment and our ADZS-USB-ICE is gone.

Can we use the new ICE2000 to program them?

I can see in the ICE2000 manual

"Multiple processor I/O voltage support: 1.8V, 2.5V, and 3.3V"

Is that 5V tolerant as USB-ICE was?

I have to decide the purchase of the ICE based on the answer to this question.

Thanks in advance

GerardSager