.ldr load to spi flalsh but not boot

I followed the Readme_Power_On_Self_Test_SC584.html in ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2 package.i have successfully generated the file Power_On_Self_Test_SC584_Cortex.ldr,and successfully to load to spi flash use cldp tool,but it cann't boot.what's the problem?

Is it the -init file not correct?The init file i used was ezkitSC584_initcode_core0_v10.
my board is :ADZS-SC584-EZLITE
package is :ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2
CCES is :CrossCore Embedded Studio 2.8.3
  • 0
    •  Analog Employees 
    on Sep 30, 2019 10:53 AM

    Hi,

    In order to assist you better on this can you please provide your comments on the below points.

    1) Can you please explain us your exact issue.
    2) Can you please confirm us whether it’s a SPI master boot?
    3) Can you please let us know whether you are getting any error.
    4) What is the boot format you are using?

    In case of booting failure, can you try adding the below loader switch in the additional options of project while creating the ldr file.
    -MaxBlockSize 0xFFFC
    There might be a block which is more than 64K and that may result to boot failure. Using this switch, the loader limits the block size to a max of 0xFFFC.

    NOTE : Use the -MaxBlockSize switch to limit the block size to a value less than 64KB. As boot code needs to be aligned on a 32-bit boundary,the maximum size of any individual block is 65,532 (0xFFFC); therefore, use -MaxBlockSize 0xFFFC in the additional options while creating the loader file.

    Regards,
    Anand Selvaraj.