Hello.
I have EV-DEMORAD24G (FMCW radar evaluation bord) which use ADSP-BF706.
For developing software, I want to know how to program the firmware into SPI flash memory.
The SPI flash memory is connected to SPI2 port of ADSP-BF706.
ADSP-BF706 boot mode is SPI2 Master.
In the circuit, USB0 port of ADSP-BF706 is connected to USB connecter.
And jtg (JTAG) port of ADSP-BF706 is directly connected to 10-pin pin header.There is no IC between jtg port and pin header.
What is recommended way to program SPI flash ROM ?
The usable port of Windows PC is only USB.
If special tool is nedded, please tell me that part number (for example, JTAG download cable).
Hi,We have Processors Software and Tools page that provides a convenient look-up table to indicate to users what evaluation platforms, extender cards, emulators, software development tools, and middleware are available for the specific processors you have chosen to evaluate for your designs.www.analog.com/.../blackfin-processors-software-and-tools.htmlPlease note that the main advantage the ICE-1000/ICE-2000 have over our older emulators is that it supports all our new processors going forward. For example, the ICE-1000 and ICE-2000 are the only emulators that support the recently launched processors (as well as all previous SHARC and Blackfin processors).Also,please refer the below FAQ to know about ICE-1000/2000.FAQ:Introducing the ADZS-ICE-1000 and ADZS-ICE-2000 Emulatorsez.analog.com/.../6740Regards,Lalitha.S
Thank you for your response.