Post Go back to editing

Verify ADSP -21584 / SC584 Clock rate

Hi

Just wont to approve the Sharc cores max clock rate.

it used to be 450Mhz and now I see in ADI site, it was update to 500Mhz.

Is it correct? Are there no heating problems?

Thanks in advance

Alon.

Parents Reply
  • Hi,

    As per the datasheet, ADSP-21584BBCZ-4A supports maximum Processor Instruction Rate of 450MHz at –40°C to +85°C . We cannot guarantee the proper operation of the devices if the specification not followed. So, we would suggest you to follow the specifications as mentioned in datasheet.

    Regards,
    Anand Selvaraj.

Children
No Data