Post Go back to editing

ADAU1462 reset and idle power consumption

Can you please advise if the datasheet power consumption figures are correct for reset and idle over TA = −40°C to +105°C.

It states the maximum is 559mA !!

http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1462-1466.pdf

Page 5

TA = 25°C

Idle State              18.3       18.7       19.9 mA     Power applied, DSP not enabled

Reset State           18.3       18.7      19.9 mA     Power applied, RESET held low

Page 6

TA = −40°C to +105°C

                             Min       Typ        Max

Idle State              5.9       15.7       559 mA     Power applied, DSP not enabled

Reset State           5.9       15.7      559 mA     Power applied, RESET held low



changed the datasheet link
[edited by: euanbrown at 1:58 AM (GMT -4) on 7 Sep 2018]