Post Go back to editing

Hybernation

Thread Summary

The user inquires about waking a Blackfin processor from hibernation using an external GPIO event. The final answer confirms it is possible and provides methods to verify hibernation mode, including measuring VDD_INT voltage or using a LED blink program. The accompanying answer suggests referring to the BF70x Blackfin Processor Hardware Reference Manual for specific wake-up sources on the BF706 processor.
AI Generated Content
Category: Hardware
Product Number: ADSP-BF706

Hi All

I am trying to put the blackfin into hybernation (or deep power down) and want to wake up from an external GPIO event.

Is that possible. Are there any engineering notes about this?

Best regards
Henrik

Parents Reply Children
  • Thanks Nandini.

    I will try to make such an implementation next week. I guess I cannot run this in debug mode, but must make a release to test upon?

  • Hi Henrik,

    You can also try this using debug mode. In deep sleep mode, once the processor wakes up, it resumes execution.

    In hibernate mode, there is no power dissipation on the VDD_INT power domain, and the processor undergoes a reset when it wakes up from hibernation.

    There are two ways to verify if the processor is in hibernate mode:

    1.Measure the VDD_INT voltage — it will be zero if the processor is in hibernate mode.
    or
    2.Load a LED blink program and observe if the processor boots and runs it correctly after waking up from hibernate mode.

    Regards,
    Nandini C

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.