Post Go back to editing

USB Resume operation failure

Category: Hardware
Product Number: ADSP-BF706BCPZ4, ADSP-BF706

Issue Description:

     We used ADSP-BF706BCPZ4 processor configured USB full speed mode and impedance 90ohm on PCB.

Added 27-ohm series resistor for USB D+ and D- line with ESD 27pF capacitance on the USB data lines.

The issue happens some randomly after the 100 to 300 times USB suspend and resume operation cycle. The USB stuck in suspend state. That means USB Data D+ line show high and Data D- show Low. the USB resume cycle is not operating and after some time the USB connection got lost and re-enumeration trying the host. But Host unable to connect with ADSP processor as device. After power reset only, it will be recovered to operate.

Could you please help to fix this.

Regards

 Palani

Thread Notes