Post Go back to editing

UART and SPI (or mayby any two non-DMA interfaces) conflict in same Blackfin 561 core

Category: Software
Product Number: ADSP-BF561
Software Version: VisualDSP++ 5.1.2.0

I try to use two interfaces to work together: UART and SPI-slave.


For the B core, I have UART initialization:

void uart_init(unsigned int divisor)
{
packet_ready = false;

com_init(divisor);

*pILAT = *pILAT | EVT_IVG8; // clear pending IVG7 and IVG8 interrupts
*pSICB_IAR3 = Peripheral_IVG(
28,
8);


*pUART_IER = ETBEI | ERBFI;

asm("ssync;");

register_handler(
ik_ivg8,
ISR_UART_receive);

*pSICB_IMASK0 |= SIC_MASK(28);
}

For the A core, I have define-switched SPI-slave initialization:

void vovka_spi_slave_init_a(void)
{
*pSPI_CTL &= (~SPE); // disable SPI
*pSPI_STAT = TXCOL | RBSY | MODF | TXE;

*pSPI_FLG = 0;

*pSPI_BAUD = SPI_BAUD_RATE_DIVISOR;

*pSPI_CTL = CPOL | PSSE | EMISO; 

asm("ssync;");

*pSPI_CTL |= SPE; // enable SPI

register_handler(
ik_ivg11,
SPI_Interrupt);
*pSICA_IAR3 = Peripheral_IVG(
27,
11);
*pILAT |= EVT_IVG11;

asm("ssync;");

*pSICA_IMASK0 |= SIC_MASK(27);

asm("ssync;");

}

Analogously, I have define-switched SPI-slave initialization for the B core:

void spi_slave_init_b(void)
{
*pSPI_CTL &= (~SPE); // disable SPI
*pSPI_STAT = TXCOL | RBSY | MODF | TXE;

*pSPI_FLG = 0;

*pSPI_BAUD = SPI_BAUD_RATE_DIVISOR;


*pSPI_CTL = CPOL | PSSE | EMISO; 

asm("ssync;");

*pSPI_CTL |= SPE; // enable SPI

register_handler(
ik_ivg11,
SPI_Interrupt);
*pSICB_IAR3 = Peripheral_IVG(
27,
11); // DMA2 Channel 4 interrupt (SPI) 27 IVG9 27
*pILAT |= EVT_IVG11; // clear pending IVG9 interrupts

asm("ssync;");

*pSICB_IMASK0 |= SIC_MASK(27);

asm("ssync;");

}

And i see the next behavior:

  • when I switch my defines to use the A-core SPI, both UART and SPI work;
  • when I switch to the B-core SPI, UART works and SPI fails, and 
  • when I use the B-core SPI without UART setup, SPI works.

The same thing could be seen when i try to compose SPI and SPORT in one core.


What should I add/change to make UART and SPI to work in the B-core?

Or maybe there is a fundamental restriction that prevents any two non-DMI interfaces to work together in one core?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.