Post Go back to editing

Permitted Clock Frequencies

Thread Summary

The user inquires about the maximum core clock frequency for different Blackfin+ processors, noting discrepancies between the datasheet and ordering guide. The support engineer confirms that the 'Processor Instruction Rate (Max)' in the ordering guide corresponds to the maximum fCCLK in Table 17 of the datasheet. For the ADSP-BF700KCPZ-1 and ADSP-BF702KCPZ-3, the user should configure the CGU registers according to the 'Ratio Restriction' in Table 17 to ensure compliance with the maximum instruction rate.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADSP-BF700

Hi,

The Blackfin+ datasheet does not have any derivative dependent clock specifications  (tables 17,18,19,28), however in the ordering guide there are different "Processor Instruction Rate (max)" values.

I would assume that these instruction rates relate at least to maximum allowable core clock frequencies, but that contradicts the specification tables (especially table 17) which do not destingush between the different processors.

So, if I use a Blackfin+ with SYS_CLKIN = 40MHz this will result in 120MHz coreclock after reset, if I understand the default/reset settings of the GCU registers correctly. Is that a valid setting for a BF700?

What restrictions apply to the clocks for those processors that cannot use a max instruction rate of 400MHz?

Parents
  • Hi Julian,

    As mentioned in the ADSP-BF70x datasheet, "The data presented in the tables applies to all speed grades (found in the Ordering Guide) except where expressly noted". You can refer the "Ratio Restriction" available in the Table 17(Page No: 50/114) and configure the CGU register as per your requirement for the processors that don't support 400MHz.

    Please let us know if you need further assistance on this.

    Regards,
    Nandini.C

  • So, I assume that "Processor Instruction Rate (Max)" in the Ordering Table is the max fCCLK in Table 17?
    "... except where expressly noted" -> I have not found any note in the whole document that states any conditions/restrictions dependent on the order code.

Reply Children