Hi,
I got a query regarding asynchronous memory writes. The problem description is given below
The following are the data regarding my system
Processor - BF527
CCLK = 122.88Mhz
SCLK = 12.288MHz (CCLK/SCLK =10)
I am using an SRAM on the asynchronous memory bank 3.
The EBIU_AMBCTL1 register is programmed with the following values
B3WAT = 0xF (Write access time - 15 cycles)
B3HT = 11(Hold time - 3 cycles)
B3ST = 11(Set up time - 3 cycles)
This means that the total SCLK required for a write is(15+3+3) = 21 SCLK or 210 CCLK
Can I perform two consecutive write operation with out any delay in the above case?
Should I give a delay of 210 CCLK in between two writes ?
Will the core waits to finish a write opeartion so that the two datas are written properly to SRAM?
Please kindly help......
Antony,
Programmer does not need to insert delays in code. There is a section called Load/Store Operation in the Programming Ref Manual that explains more on this ::-
In write operations, the store instruction is considered complete as soon as it executes, even though many cycles may execute before the data is actuallywritten to an external memory or I/O location. This arrangement allows the processor to execute one instruction per clock cycle, and it implies that the synchronization between when writes complete and when subsequent instructions execute is not guaranteed. Moreover, this synchronization is considered unimportant in the context of most memory operations.
Regards
Prasanth..
Dear Presanth,
What happens if the next instruction that follows the async memory read uses the same data that is read from memory?
Hi Antony,
That is where the idea of 'interlocked-pipeline' comes from, which is a mechanism to resolve the R/W hazards. Simplest way to put it - processor pipeline is locked until data is 'actually' read from memory.
This is also explained in the document section I mentioned earlier:-
In the execution of instructions, the Blackfin processor architecture implements an interlocked pipeline. When a load instruction executes, the
target register of the read operation is marked as busy until the value is returned from the memory system. If a subsequent instruction tries to
access this register before the new value is present, the pipeline will stall until the memory operation completes. This stall guarantees that instructions
that require the use of data resulting from the load do not use the previous or invalid data in the register, even though instructions are allowed to start execution before the memory read completes.
Also the info in section 'Ordering of Loads and Stores' is very important to understand the ordering of read & write operations.
Prasanth.
Thanks for the support
Dear Presanth:
How can I reduce the delay between two asynchronous memory reads?