Post Go back to editing

Delay between Asynchronous memory writes/reads

Hi,

I got a query regarding asynchronous memory writes. The problem description is given below

The following are the data regarding my system

Processor - BF527

CCLK = 122.88Mhz

SCLK = 12.288MHz (CCLK/SCLK =10)

I am using an SRAM on the asynchronous memory bank 3.

The EBIU_AMBCTL1 register is programmed with the following values

B3WAT = 0xF (Write access time - 15 cycles)

B3HT = 11(Hold time - 3 cycles)

B3ST = 11(Set up time - 3 cycles)

 

This means that the total SCLK required for a write is(15+3+3) =  21 SCLK or 210 CCLK

 

Can I perform two consecutive write operation with out any delay in the above case?

Should I give a delay of 210 CCLK in between two writes ?

Will the core waits to finish a write opeartion so that the two datas are written properly to SRAM?

 

Please kindly help......

 

Parents
  • Antony,

    Programmer does not need to insert delays in code. There is a section called  Load/Store Operation in the Programming Ref Manual that explains more on this ::-

    In write operations, the store instruction is considered complete as soon as it executes, even though many cycles may execute before the data is actually
    written to an external memory or I/O location. This arrangement allows the processor to execute one instruction per clock cycle, and it implies that the synchronization between when writes complete and when subsequent instructions execute is not guaranteed. Moreover, this synchronization is considered unimportant in the context of most memory operations.

    Regards

    Prasanth.
    .

Reply
  • Antony,

    Programmer does not need to insert delays in code. There is a section called  Load/Store Operation in the Programming Ref Manual that explains more on this ::-

    In write operations, the store instruction is considered complete as soon as it executes, even though many cycles may execute before the data is actually
    written to an external memory or I/O location. This arrangement allows the processor to execute one instruction per clock cycle, and it implies that the synchronization between when writes complete and when subsequent instructions execute is not guaranteed. Moreover, this synchronization is considered unimportant in the context of most memory operations.

    Regards

    Prasanth.
    .

Children
No Data