Post Go back to editing

Powering Circuit Q's

Hello,

I am have some questions regarding the Schematics of the BF548 ezkit (attached). Specifically

the powering sections.

Firstly, a basic questions, what is the difference between the filled square and hollow

circle schematic symbol for the power buses? The page Power Page 1, for example,

on the bottom right shows the circuitry for the VDDEXT and 3.3V, shown as filled square

and hollow circle respectively. They are both 3.3V so what is the difference?

Looking now at Power Page 2, I don't really understand the power supply for VDDDR and

5V. What does the adp1823 chip setup do? I looked briefly at its datasheet but didn't

understand how it relates to the regulation of VDDDR and 5V (again the symbols are different?).

On the bottom left of this page there are two outputs for 5V_USB? Why?

Also, on the bottom right there are these symbols (MH4, MH5, etc) but they aren't connected

to anything? What are they for?

It's pretty evident there are lots of things that I'm confused with - the power circuitry has been

a bit of a hurdle. Is there an easier design for the power supply? Would really appreciate

any reference designs that have a simpler powering system.

Thanks to anyone who can be bothered to try and help. I know it is not exactly 'fun', but it

will be much appreciated.

Cheers...

A0206-2006_CUST.pdf
Parents
  • Hi dlh,

    Sorry if I misspelled you name before.

    Yes you are correct. The Zener is about 2.2V.  The forward drop of D7 is only .3V.  Likewise D2 drops the 3.6V supply to 3.3V when the device is operational.  The unpowered voltage may be closer to 2.5V than to 3V.  That’s ok because you are not operating the device.  The processor is powered off and you do not need the minimum 3.0V.  Even less than 2V should prevent any damage caused by ageing.  Before I said months of ageing at worst-case temperature.  That was conservative.  We know of no failures.

    I have not studied the noise on VBUS.  Don’t quote me but I think there may be a maximum inrush current spec for USB VBUS.  If I remember correctly, that limits you to about 10 or 15uF.

    Thanks for you interest.

    _BobK

Reply
  • Hi dlh,

    Sorry if I misspelled you name before.

    Yes you are correct. The Zener is about 2.2V.  The forward drop of D7 is only .3V.  Likewise D2 drops the 3.6V supply to 3.3V when the device is operational.  The unpowered voltage may be closer to 2.5V than to 3V.  That’s ok because you are not operating the device.  The processor is powered off and you do not need the minimum 3.0V.  Even less than 2V should prevent any damage caused by ageing.  Before I said months of ageing at worst-case temperature.  That was conservative.  We know of no failures.

    I have not studied the noise on VBUS.  Don’t quote me but I think there may be a maximum inrush current spec for USB VBUS.  If I remember correctly, that limits you to about 10 or 15uF.

    Thanks for you interest.

    _BobK

Children
No Data