Post Go back to editing

Powering Circuit Q's

Hello,

I am have some questions regarding the Schematics of the BF548 ezkit (attached). Specifically

the powering sections.

Firstly, a basic questions, what is the difference between the filled square and hollow

circle schematic symbol for the power buses? The page Power Page 1, for example,

on the bottom right shows the circuitry for the VDDEXT and 3.3V, shown as filled square

and hollow circle respectively. They are both 3.3V so what is the difference?

Looking now at Power Page 2, I don't really understand the power supply for VDDDR and

5V. What does the adp1823 chip setup do? I looked briefly at its datasheet but didn't

understand how it relates to the regulation of VDDDR and 5V (again the symbols are different?).

On the bottom left of this page there are two outputs for 5V_USB? Why?

Also, on the bottom right there are these symbols (MH4, MH5, etc) but they aren't connected

to anything? What are they for?

It's pretty evident there are lots of things that I'm confused with - the power circuitry has been

a bit of a hurdle. Is there an easier design for the power supply? Would really appreciate

any reference designs that have a simpler powering system.

Thanks to anyone who can be bothered to try and help. I know it is not exactly 'fun', but it

will be much appreciated.

Cheers...

A0206-2006_CUST.pdf
Parents
  • Thanks a lot for the detailed response..

    Regarding the power specialists, do they provide free support / power design advice? This could be very helpful.

    I would like to know whether the powering circuit could be simplified if the complexity/functionality of the system

    is much simpler than the bf548 ezkit. For example, if we didn't have a hdd in the system could it save some

    power circuitry etc..

    Thanks again..

Reply
  • Thanks a lot for the detailed response..

    Regarding the power specialists, do they provide free support / power design advice? This could be very helpful.

    I would like to know whether the powering circuit could be simplified if the complexity/functionality of the system

    is much simpler than the bf548 ezkit. For example, if we didn't have a hdd in the system could it save some

    power circuitry etc..

    Thanks again..

Children
No Data