Post Go back to editing

Blackfin BF561 interface with AD6654

I am using Blackfin BF561 EZ kit to interface AD6654. I made a custom board for ad6654. I am trying to program ad66654 through microport.  to test the setup i have written small program that is testing wrting and reading some address locations of AD6654. but i am not able to read and write these location.

My interface is as follows -

Blackfin                AD6654

Adress( 9 -2)        Adress( 7 -  0 )

Aata ( 15 -0)         Data( 15 -  0 )

SCLK1                 CPUCLK

SMODE              logic 0

Mode                  logic 0

WR\                   AWE\                

RD\                    AOE\

CS\                   AMS1\

I am using bank1 asynchronous memory interface. SCLK1 is about 60MHz. My code is attached for review. Please suggest.

Thanks in Advance

code.txt.zip
Parents Reply Children
No Data