What is the procedure to erase and program ADZS-BF527-EZKIT LITE eval board?

Hi,

  Recently i purchased ADZS-BF527-EZKIT LITE eval board. I was able to install Visual DSP++5.0 (90 days evaluation) software and wrote a small C code to blink an LED. I am able to build the program successfully and it also shows load completed successfully (.dxe file). I am not able to blink LED and will still execute the default program tat has come along with eval board. I feel i am not able to properly load the program. Is there any way to erase the previous program. I couldnt find any option for erasing program. Please help me.

Thanks and Regards,

Shilpa

Parents
  • I am using Visual DSP++ 5.0. There is no folder with the name  ADSP-BF527 EZ-KIT Lite in the path as you told  ........\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF527 EZ-KIT Lite\Flash Programmer. I can only see folders with BF533, BF535, BF537 and BF538 If possible please share me the folder i.e, zip it and send as attachment.


Reply
  • I am using Visual DSP++ 5.0. There is no folder with the name  ADSP-BF527 EZ-KIT Lite in the path as you told  ........\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF527 EZ-KIT Lite\Flash Programmer. I can only see folders with BF533, BF535, BF537 and BF538 If possible please share me the folder i.e, zip it and send as attachment.


Children
No Data