Post Go back to editing

Booting Issue?

Category: Software
Product Number: blackfin 609
Software Version: CCES2.11

Hi 

Can Anyone Help me with this Error...

I Flashed Some Application Code ,Application Code Has Some peripherals like (UART,SPI,SPORT,SMC) Flashed with SPI quad . After Completion Of Flash, Custom board was Turned Off and Turned On But booting was Not happened.

I tried to Debug that Application Code with EMULATOR  ICE -2000 ,The Process was  Reaching 70% after That CCES was Not Responding

I'm Not Using DDR2(DMC).

Parents Reply Children
  • Hi Shiva,

    There could be a possibility of application getting corrupted during flashing.

    Can you provide some more information to narrow down the issue you might be facing:

    1. Does this issue occur every time you try to Debug the application after flashing?
    2.  Did you check your board in boot mode 0 and try booting with a simple LED blink code to check if the system behaves correctly?
    3. Did you run the ICE Test utility and determine the JTAG connection every time it fails?

    Let us know if the custom boards have any issues even while debugging with a simple LED code and you are facing same issues then?


    Regards,
    Divya.P

  • Hi Divya,

    After This Iteration 

    1.  Did you check your board in boot mode 0 and try booting with a simple LED blink code to check if the system behaves correctly?
    2. Did you run the ICE Test utility and determine the JTAG connection every time it fails?

    It's working Fine.

    Thank you for your Support!

    Best Regards ,

    ShivaChary.