error

Error: no section in the code memory space

Tool failed with exit/exception code: 4294967295...im getting this error while compiling my code for ADSPBF512 .Im new to blackfin programming.Please guide me on what all i should check to trouble shoot this error

Parents
  • Hi,

    you say you are using the DXE for the BF512 - is it possible that you are selecting the file "...\Blackfin\ldr\ADSP-BF512-ROM-V0*.dxe" as your Init Code file? Note that this file is the Boot ROM code, not an init code file.

    The only example Init Code we provide for the BF51x family is for the BF518F EZ-KIT Lite. This is found at "...\Blackfin\ldr\ezboardBF518f_initcode_ROM-V0*.dxe".

    This init code is specific for the BF518, and for the SDRAM part used on that EZ-KIT Lite. You will find the example project file at "...\Blackfin\ldr\init_code\c\ADSP-BF518F EZ-Board\", you should make a copy of this file, and any required source files from the "...\Blackfin\ldr\init_code\c\src\" directory, and edit them to create a new Init Code suitable for your custom target.

    Regards,

    Craig.

Reply
  • Hi,

    you say you are using the DXE for the BF512 - is it possible that you are selecting the file "...\Blackfin\ldr\ADSP-BF512-ROM-V0*.dxe" as your Init Code file? Note that this file is the Boot ROM code, not an init code file.

    The only example Init Code we provide for the BF51x family is for the BF518F EZ-KIT Lite. This is found at "...\Blackfin\ldr\ezboardBF518f_initcode_ROM-V0*.dxe".

    This init code is specific for the BF518, and for the SDRAM part used on that EZ-KIT Lite. You will find the example project file at "...\Blackfin\ldr\init_code\c\ADSP-BF518F EZ-Board\", you should make a copy of this file, and any required source files from the "...\Blackfin\ldr\init_code\c\src\" directory, and edit them to create a new Init Code suitable for your custom target.

    Regards,

    Craig.

Children
No Data