ADSP-BF533 EZ-KIT Lite  AD1836

Hello ereryone, i'm a  freshman about bf533.now i'm faced a problem which confule me  about one weeked. that is: I want use the  sport0'Rx and spi'Rx port to receive two group of  datas. then employ subtraction on these two group datas  after the two group data was normalizated. in order not to lose data, i use pingpong method.  the  bf533 EZ-KIT Lite  has 4  input jarks and 6 output jarks. now my queston is  how i  can discriminate  the input jarks.  how i  konw the  spi  input jack   and   sport0 input jark. i has read the visul dsp++'s example ,the project is C_Talkthrough_TDM.  what functon about    iChannel0LeftIn  iChannel0RightOut in project.  hope  have explain the problem clearly .who can help me,thank you vevy much.

Parents Reply
  • 0
    •  Analog Employees 
    on Nov 8, 2019 11:35 AM in reply to Thanh Nguyen

    Hi Thanh,

    We would suggest you to look at the POST Example provided in the below installation directory of VDSP++.
    (Installation_Directory)\Analog Devices\VisualDSP 5.1.2\Blackfin\Examples\ADSP-BF533 EZ-KIT Lite\Power_On_Self_Test

    If you are using the CCES Software for Developing, we would suggest you to download the ADSP-BF533 Board Support Package (BSP) from the below link and install it your PC. Once you installed , you can find the example codes for BF533.

    BSP Link :www.analog.com/.../BF533-EZLITE.html

    (Installation_Directory)\Analog Devices\ADSP-BF533_EZKIT-Rel1.0.1\BF533_EZ-Kit_Lite\Blackfin\Examples

    Regards,
    Anand Selvaraj.

Children
No Data