Post Go back to editing

BF512, PPI, DMA0 and AD7622 adc

I am trying to use System Services to operate an AD7622 A/D converter.  The ADC is connected to the PPI and I have programmed the DMA.  I have connected the AD7622's BUSY signal to the BlackFin's DMAR0 (PG2) pin.  I can not find an adi_dma_Control() command to specify that I am using DMAR0.  Both the PORTG_MUX and PORTG_FER registers have the wrong values.  Here is my initialization code:

- - - - - - - - - -

   ADI_DMA_MANAGER_HANDLE  dmaHandle;

   ADI_DCB_HANDLE          dcbPpiServer;

   ADI_DMA_CHANNEL_HANDLE  pDmaPpiChannelHandle;

   ADI_DMA_RESULT          dma_result;

   ADI_DMA_CONFIG_REG      dma_config_register;


   dmaResult = adi_dma_Init (&dmaManager_workspace, DMA_MGR_WS,

                             &dmaDevices, &dmaHandle,

                             &dmaCriticalRegionArg);

   dma_result = adi_dma_Open (dmaHandle,

                              ADI_DMA_DMA0,   // DMA 0 - default for PPI.

                              NULL,

                              & pDmaPpiChannelHandle,

                              ADI_DMA_MODE_CIRCULAR,

                              dcbPpiServer,

                              copy_buffer);

    /* Circular; Call back on sub-buffer complete */

    dma_config_register.b_DMA2D  = ADI_DMA_DMA2D_LINEAR;

    dma_config_register.b_NDSIZE = ADI_DMA_NDSIZE_STOP;

    dma_config_register.b_WDSIZE = ADI_DMA_WDSIZE_16BIT;

    dma_config_register.b_DI_SEL = ADI_DMA_DI_SEL_INNER_LOOP;

    dma_config_register.b_DI_EN  = ADI_DMA_DI_EN_ENABLE;

    dma_config_register.b_WNR    = ADI_DMA_WNR_WRITE;

    dma_config_register.b_FLOW   = ADI_DMA_FLOW_AUTOBUFFER;

   dma_result = adi_dma_Buffer(pDmaPpiChannelHandle,

                               pingPong,

                               dma_config_register,

                               ARRAY_SIZE,

                               2u,         /* 2 Bytes = 16-bit datum */

                               2u,         /* 2 sub-buffers */

                               0u);        /* Ignored value */

  dma_result = adi_dma_Control (pDmaPpiChannelHandle,

                                ADI_DMA_CMD_SET_DATAFLOW,

                                DMA_ENABLE);

- - - - - - - - - -

I suspect I am NOT doing some needed initialization, but I am stumped.  Any ideas?  Thanks.

Regards,

Fred