Post Go back to editing

BF548:  LAN9218 driver

I need to rebuild the LAN9218 driver with the base address changed.   I do not see the LAN9218 driver source code inside the C:\Program Files\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF548 EZ-KIT Lite

Is the source available somewhere? 

ELse is there a way to change the base address without compiling the driver again??

Thanks in advance

Krishna

Parents
  • Hi,

    What changes have you made to the example applications, or Template applications to account for the changes in the custom driver, and to ensure the correct driver is included in the project (rather than the default)?

    Are you able to provide a complete example project setup - for example using the LwIP template application - and your library so that we can take a closer look?

    Regards,

    Craig.

Reply
  • Hi,

    What changes have you made to the example applications, or Template applications to account for the changes in the custom driver, and to ensure the correct driver is included in the project (rather than the default)?

    Are you able to provide a complete example project setup - for example using the LwIP template application - and your library so that we can take a closer look?

    Regards,

    Craig.

Children
No Data