Post Go back to editing

CLDP Reprorted done but code is not executing from spi flash when change Boot Mode 3 to Spimaster and pressed reset.

Category: Software
Product Number: ADSP-BF609 EZ BOARD
Software Version: 1.0

I have written a toggle LED code in Core 0 and executed in .dxe its working well.

I I want to boot this toggle code from spi flash,so I followed steps:

1)Generated a loader file:
•  Project: Properties: C/C++ Build: Settings. In the 'Build Artifact' tab set the 'Artifact Type' to "Loader File".

• Back under the "Tools Settings" tab, go to the 'CrossCore Blackfin Loader' settings and, under 'General' set:

• Boot Mode: "SPI Master"

• Boot Format: "Intel Hex"

• Output Width: 8

• In the "Initialization File" field, browse to the "BF609_init_v00.dxe" file in the CrossCore Embedded Studio installation under "...\Blackfin\ldr\".

• Boot code(-bcode):0x1

• Rebuilded and I generated .ldr file 

2)I have loaded .ldr file in spi flash using CLDP:

      cldp -proc ADSP-BF609 -emu KIT -driver "C:\Analog Devices\ADSP-BF609_Evaluation_Board-Rel1.1.0\BF609_EZ-Board\Blackfin\Examples\Device_Programmer\serial\bf609_w25q32bv_dpia.dxe" -cmd prog -erase affected -format hex -file "D:\codes\tog_Core0\Debug\tog_Core0.ldr"

3)CLDP reported done



4)But when I have change Boot Mode to 3(0111) and pressed reset button my code is not executing.


 Help me in this if I have missed any configuration.