Hello, everyone
I use ICE-1000 emulator for debugging dsp BF-606 code. I've got BF-606 and connected ADC AD7817 via SPI. The code is developed in Cross Core Embedded Studio 1.2. The problem is the following: when using ICE-1000 (expression window is used to browse variables) the data from ADC is invalid (from time to time I get 0 code in my variable instead of something meaningful). However, I didn't catch any zero code with the help of oscilloscope.
BF-606 connected to flash memory, I loaded code to the flash memory via UART. When BF-606 executes code from flash memory everything goes well. So, my question is: Is there anybody who face similar problem with ICE-1000? Can it be connected with using Cross Core without valid license.
Thanks.