Post Go back to editing

ADSP-BF533 Oscillator Change Out

I'm changing out the U11 12.288MHz oscillator on the ADSP-BF533 for a different frequency. As you can see from the picture, I had a pretty clean removal of the old oscillator. The interesting thing is that the top two pads (1 & 2) both have continuity when I check it against ground and in return have continuity with each other. This seems unusual to me. Do I have another problem?