Post Go back to editing

How to check the processor version at runtime?

Thread Summary

The user asked how to detect the processor version (BF700 to BF707 or BF607 to BF609) at runtime for a mixed hardware setup connected via SPI. The solution involves checking the REVID bits <31:28> of the TAPC0_IDCODE register for BF70x processors and the SDU_IDCODE register for BF60x processors to identify the specific processor type.
AI Generated Content

How to check, at runtime, the version of the processor?

Is there a register or Rom function/variable that holds an ID of the type being a BF700 -> BF707?
Same issue on BF60x.

On my current project, the hardware can be a mix of BF706/BF709 and/or BF607/BF609 processors connected through SPI ports to a host processor.

I like to detect the dsp type by uploading an dxe that can communicate back the correct version.

After this the host processor can start booting the main firmware image, compiled for the correct DSP.

bf70x bf60x

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.