Post Go back to editing

EVAL-BF538F-EZLITE

JTAG Description:

Hello, will this connector be compatible with ADZS-USB-ICE JATG Programmer? 

Provide Part No. or Mechanical dimensions of connector as well.

Our DSP Part no. is ADSP-BF538BBCZ-4F8

Parents
  • Hi Nikhil26,

    I moved this to Blackfin Processors community. Someone here should be able to help.

  • Hi,

    We recommend to refer the EE-note(EE-68) for more details on JTAG  emulator  interface.This document provides technical information to properly design a JTAG emulator interface for Analog Devices, Inc (ADI) processor targets.

    We would suggest you to refer the Figure 4.JTAG HPUSB JTAG emulator pod dimensions (Page No:5/20). The link for the Analog Devices JTAG Emulation Technical Reference (EE-68) is given below.
    www.analog.com/.../ee-68.pdf

    Please let us know if you need any further assistance.

    Regards,
    Anand Selvaraj.

  • The technical (EE-68) tells the connector specification as " The JTAG emulator target header interface is a standard dual-row 0.025” male square-post header, employing 0.1” x 0.1” spacing, with a minimum post length of 0.235” "

    I'm trying to understand the above JTAG Target Header Specification :

    JTAG header should be

    1. Dual Row = 7 pins on each row

    2. Pitch should be 0.1'' (or 2.54mm)

    3. 0.025'' contact pin dimension - 0.635mm x 0.635mm

    4. Min Post length of 0.235'' - pin height to be a minimum of 5.97mm

      Is my above understanding right? Please let me know as I need to select a target header for on board ADSP-BF538BBCZ-4F8.

Reply
  • The technical (EE-68) tells the connector specification as " The JTAG emulator target header interface is a standard dual-row 0.025” male square-post header, employing 0.1” x 0.1” spacing, with a minimum post length of 0.235” "

    I'm trying to understand the above JTAG Target Header Specification :

    JTAG header should be

    1. Dual Row = 7 pins on each row

    2. Pitch should be 0.1'' (or 2.54mm)

    3. 0.025'' contact pin dimension - 0.635mm x 0.635mm

    4. Min Post length of 0.235'' - pin height to be a minimum of 5.97mm

      Is my above understanding right? Please let me know as I need to select a target header for on board ADSP-BF538BBCZ-4F8.

Children