Post Go back to editing

ADSP-BF518F EZ-Board expansion interface

The schematic of ADSP-BF518F EZ-Board shows P2 and P4 connectors are the same. Is this an error on the schematics?

Parents
  • Hello Guang,

    Note that all the GPIO pins has multiplexed functionality. For instance, as you can see in the below image the pin 159 has multiplexed functionality  like PH3/DT1/SPI1_MOSI_RSI_DATA7 marked inside U12 layout. The node which is connected to this pin is available on the P2 expansion interface. So it implies that you could use P2.25 as SPI1_MOSI pin. Similarly the P4.25 can be used as SPI0_MOSI.

     Exerpt from ADSP-BF518 (U12) page# 92/110: 

    Exerpt from Expansion interface P2 page# 102/110:

      

    Hope this clears your doubt.

    Best Regards,

    Jithul

Reply
  • Hello Guang,

    Note that all the GPIO pins has multiplexed functionality. For instance, as you can see in the below image the pin 159 has multiplexed functionality  like PH3/DT1/SPI1_MOSI_RSI_DATA7 marked inside U12 layout. The node which is connected to this pin is available on the P2 expansion interface. So it implies that you could use P2.25 as SPI1_MOSI pin. Similarly the P4.25 can be used as SPI0_MOSI.

     Exerpt from ADSP-BF518 (U12) page# 92/110: 

    Exerpt from Expansion interface P2 page# 102/110:

      

    Hope this clears your doubt.

    Best Regards,

    Jithul

Children
No Data