Post Go back to editing

ADSP-bf 609 upgrade using uart rs 232

hi,

I'm new to bf 609 ;

I want to load the program in baremetal using rs 232

IN C0RE 0 +CORE1 I WANT TO FLASH THE PROGRAM USING RS 232

I USE  THIS METHOD ALSO , Didn"t  correct answer in the console,

ADSP-SC58x Firmware Upgrade using UART

Attached is the ADSP-SC58x example code for firmware upgrade via UART along with multiple loader streams. Also the attached ADSP-SC58x_UART_Firmware_Upgrade.pdf document contains the procedure to upgrade the firmware.
 We tired this method in bf 609 .
we got real term application