hi,
I'm new to bf 609 ;
I want to load the program in baremetal using rs 232
IN C0RE 0 +CORE1 I WANT TO FLASH THE PROGRAM USING RS 232
I USE THIS METHOD ALSO , Didn"t correct answer in the console,
ADSP-SC58x Firmware Upgrade using UART
Attached is the ADSP-SC58x example code for firmware upgrade via UART along with multiple loader streams. Also the attached ADSP-SC58x_UART_Firmware_Upgrade.pdf document contains the procedure to upgrade the firmware.
We tired this method in bf 609 .
we got real term application