Hi,
I am trying to initializing a ST7789 controller built in a LCD in SPI mode. To do that I use SPI1 from BF706 kit board. Signals are connected as:
BF706 kit board | LCD, ST7789 |
SPI1_CLK | DCX |
SPI1_MOSI | SDA |
SPI1_MISO | SDO |
SPI1_SS | CSX |
In system.svc I set PPI and SPI1 as follow:
and I use adi_initpinmux() function to initialize the SPI1 registers.
int32_t adi_initpinmux(void) { /* PORTx_MUX registers */ *pREG_PORTA_MUX = PPI0_FS1_PORTA_MUX | PPI0_FS2_PORTA_MUX | PPI0_FS3_PORTA_MUX | PPI0_CLK_PORTA_MUX | PPI0_D08_PORTA_MUX | PPI0_D09_PORTA_MUX | PPI0_D10_PORTA_MUX | PPI0_D11_PORTA_MUX | SPI1_CLK_PORTA_MUX | SPI1_MISO_PORTA_MUX | SPI1_MOSI_PORTA_MUX | SPI1_SEL1_PORTA_MUX; *pREG_PORTB_MUX = PPI0_D00_PORTB_MUX | PPI0_D01_PORTB_MUX | PPI0_D02_PORTB_MUX | PPI0_D03_PORTB_MUX | PPI0_D04_PORTB_MUX | PPI0_D05_PORTB_MUX | PPI0_D06_PORTB_MUX | PPI0_D07_PORTB_MUX | PPI0_D16_PORTB_MUX | PPI0_D17_PORTB_MUX; *pREG_PORTC_MUX = PPI0_D12_PORTC_MUX | PPI0_D13_PORTC_MUX | PPI0_D14_PORTC_MUX | PPI0_D15_PORTC_MUX; /* PORTx_FER registers */ *pREG_PORTA_FER = PPI0_FS1_PORTA_FER | PPI0_FS2_PORTA_FER | PPI0_FS3_PORTA_FER | PPI0_CLK_PORTA_FER | PPI0_D08_PORTA_FER | PPI0_D09_PORTA_FER | PPI0_D10_PORTA_FER | PPI0_D11_PORTA_FER | SPI1_CLK_PORTA_FER | SPI1_MISO_PORTA_FER | SPI1_MOSI_PORTA_FER | SPI1_SEL1_PORTA_FER; *pREG_PORTB_FER = PPI0_D00_PORTB_FER | PPI0_D01_PORTB_FER | PPI0_D02_PORTB_FER | PPI0_D03_PORTB_FER | PPI0_D04_PORTB_FER | PPI0_D05_PORTB_FER | PPI0_D06_PORTB_FER | PPI0_D07_PORTB_FER | PPI0_D16_PORTB_FER | PPI0_D17_PORTB_FER; *pREG_PORTC_FER = PPI0_D12_PORTC_FER | PPI0_D13_PORTC_FER | PPI0_D14_PORTC_FER | PPI0_D15_PORTC_FER; return 0; }
and then using Init_SPI1() to define rest of SPI1 registers:
void Init_SPI(void) { *pREG_SPI1_CLK = 24; *pREG_SPI1_DLY = 0; //((1 << BITP_SPI_DLY_STOP) & BITM_SPI_DLY_STOP) ; *pREG_SPI1_SLVSEL= ENUM_SPI_SLVSEL_SSEL1_HI | ENUM_SPI_SLVSEL_SSEL1_EN; *pREG_SPI1_CTL = ENUM_SPI_CTL_MASTER; *pREG_SPI1_TXCTL = ENUM_SPI_TXCTL_TTI_EN | ENUM_SPI_TXCTL_TWC_EN | ENUM_SPI_TXCTL_ZERO ; *pREG_SPI1_RXCTL = ENUM_SPI_RXCTL_OVERWRITE; *pREG_SPI1_TFIFO = ENUM_SPI_TXCTL_TDR_EMPTY; *pREG_SPI1_TXCTL |= ENUM_SPI_TXCTL_TX_EN; // enable Tx SPI *pREG_SPI1_RXCTL |= ENUM_SPI_RXCTL_RX_EN; // enable Rx SPI *pREG_SPI1_CTL |= ENUM_SPI_CTL_EN; }
When I enable the SPI1 by calling "*pREG_SPI1_CTL |= ENUM_SPI_CTL_EN;", there is no signal for SPI1 clock on scope.
void Configure_LCD(void) { Init_SPI(); *pREG_SPI1_SLVSEL &= ~ENUM_SPI_SLVSEL_SSEL1_HI ; // select device *pREG_SPI1_SLVSEL &= ~ENUM_SPI_SLVSEL_SSEL1_HI ; // select device *pREG_SPI1_CTL |= ENUM_SPI_CTL_EN; //------------ST7789V SPI Initialization--------------------// device_access_short(0x01); // Command ID delay(200); //----------------------------------------------------------// *pREG_SPI1_SLVSEL &= ~ENUM_SPI_SLVSEL_SSEL1_LO ; // select device *pREG_SPI1_SLVSEL &= ~ENUM_SPI_SLVSEL_SSEL1_LO ; // select device *pREG_SPI1_CTL |= ENUM_SPI_CTL_EN; device_access_short(0x11); // Command ID delay(120); // 120ms ....... }
I am trying also to write data and command after ENUM_SPI_SLVSEL_SSEL1 is high or low. But still SPI1 is not clocking.
Anyone could please have a look at the code and explain to me what I am doing wrong.
Thank you
The data's will be write when SCL (DCX) is High and the commands will be write when DCX (SCL) is Low. How can I separate the CLK to be H and L?
[edited by: SVA at 8:31 AM (GMT -4) on 21 Sep 2020]