Hi,
In my bootloader, it is possible to write a ldr file in flash and boot the file from flash by calling "adi_rom_Boot((void *)0x40010000, 0, 0, 0, 0x207)" and it works fine. But the size of the ldr file is now more than 64K and it is not possible anymore to boot to the application when I call the same command. Do I need a precondition when I write to the two blocks in flash?
Using BF706
Thanks
New
[edited by: SVA at 9:11 AM (GMT 0) on 2 Jun 2020]