How to convert a Visual DSP project to CCES project

Hi i am having a visual dsp example project and i want to run it in CCES, can i just copy the source code to CCES and compile it ? My project i need to convert is:

C:\Program Files (x86)\Analog Devices\VisualDSP 5.1.2\Blackfin\Examples\ADSP-BF533 EZ-KIT Lite\LED Blink (C)

  • 0
    •  Analog Employees 
    on Apr 16, 2020 2:21 PM

    Hi Thanh,

    Please find the CCES examples from the ADSP-BF533 board support package. You can download and install the BSP (Board support package) for ADSP-BF533 in the below link.
    download.analog.com/.../ADI_ADSP-BF533_EZKIT-Rel1.0.1.exe

    Once you installed, you can find the example code from the below mentioned installation path.
    [Installation Directory]:\Analog Devices\ADSP-BF533_EZKIT-Rel1.0.1\BF533_EZ-Kit_Lite\Blackfin\Examples

    Regarding the code conversion from VDSP to CCES.
    >> While migrating from VDSP to CCES, there are a number of ways in which VisualDSP++ applications differ from CCES applications: RTOS, interrupt handling, SSL/DD APIs, and more. If your VisualDSP++ application uses such mechanisms, you have to make corresponding changes to your application's source code before the application can build in CCES. Similarly, if your application uses a customized LDF, the LDF may make references to libraries that are not used in CCES, or omit ones that are.

    More information about importing VisualDSP++ project files into CrossCore Embedded Studio is available at:
    ez.analog.com/.../faq-importing-visualdsp-project-files-to-crosscore-embedded-studio

    We would also recommend reading the Getting Started with CrossCore Embedded Studio FAQ:
    ez.analog.com/.../crosscore-embedded-studio-getting-started

    We have a number of CCES introductory videos on our Analog Devices Video Channel. These videos are also indexed on the CrossCore Embedded Studio product page.
    www.analog.com/.../adswt-cces.html

    Regards,
    Anand Selvaraj.