Good morningAre all the silicon rev of the ADSP-BF522 compatible with NOR serial 24-bit address flashes?Thanks
Alessandro
Hi Alessandro,In order to assist you better on this, can you please share the exact part number of the NOR serial flashes you are using. Regards,Anand Selvaraj.
Thank you for reply
I'm using ADESTO AT45DB161E. It is configured in "Power of 2" for 24bit address.
In our custom board we have actually ADSP-BF522BBCZ-4A silicon rev 0.2 configured for BOOT from SPI.
My doubt is only about other silicon rev of the ADSP-BF522 that we could buy, it would be nice to be able to confirm that other revs also have compatibility.
Thanks in advance
Any news about my question?
Hi Alessandro,Apologies for the delay.I reviewed the ADESTO AT45DB161E flash and seems that it is compatible with the ADSP-BF522 processor. Also other silicon revisions of the ADSP-BF522 processors are compatible with the flash part you have mentioned. Regards,Anand Selvaraj.