Post Go back to editing

Re: BF548 EZ-KIT Lite - USB Mass Storage Device Demo

HI martin ,

i got a problem that, when i were using the on board RAM(size is 64MB) as the mass storage in the mass_storage _app then it enumerates the board as a mass storage device(like a usb pen drive), 1.HOWEVER when i copy a file other than .txt extension i.e like a .pdf/.ppt/.doc file then it does not copy to RAM successfully.(it creates a object of that type but the actual content/size  is always zero).
2. AFTER COPYING ONE TEXT FILE THEN I AM UNABLE TO COPY ANOTHER TEXT FILE IN IT.
3.The pc enumerates the board as a 8MB pen drive, is there any method to increase the size /capacity as i have a RAM of size 64MB.

4The format and copying progress option (which normally work well with pendrivs is not working with it) it shows copying for a long time but the progress bar/details do not show the extent of copying completed.

Parents Reply Children
No Data