A 16T/16R X-Band Direct Sampling Phased Array Subsystem using Apollo MxFE

    Join our webinar on the Quad Apollo Platform, a cutting-edge solution for accelerating high-performance digital beamforming. Discover the ADXBAND16EBZ...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

     

    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

    Latest Blogs

    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
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
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents ADSP-BF70x application cannot boot using Secure Boot
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • ADSP BF706 Ezkit Mini SPI1 cannot be done in master mode.
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?
  • BF707 SPI Slave to Master loopback communication
  • Example for UART transmit and receive operation using Core Mode for BF707
  • GPIO example code for BF707
  • Hardware Reset using Watchdog in BF706
  • SPI example in Autobuffer mode on BF707

ADSP-BF70x application cannot boot using Secure Boot

Revision Creation Date Revision Author
Current Revision 27 Feb 2024 11:50 AM stephenv
Revision #3 27 Jul 2022 11:55 AM Sara Collins
Revision #2 4 Jun 2018 12:31 PM ADIApproved
Revision #1 14 May 2018 5:20 PM ADIApproved
  • Compare Versions View current version