Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation

In Dual Buffer descriptor mode, each descriptor can transfer the data from two different buffers with buffer size up to 4096 bytes. In this mode IDMAC can either use only one descriptor to transfer the data from two buffer or it can have multiple descriptors which can be chained to run one after the other. Unlike the chained descriptor mode where the descriptor has the address of next descriptor, dual buffer mode links the descriptors using a fixed offset between the end address of current descriptor and start address of next descriptor. This fixed offset is same for all the descriptors in the chain and is programmed in DSL(Descriptor Skip Length) field of MSI_BUSMOD register.

Forming a ring chain of descriptors in dual buffer mode is also possible. This is helpful if the same set of descriptors need to be used again and again in a ring form. In order to configure the IDMAC descriptors in Dual buffer ring mode, use following steps:

  • Set up the 'N' IDMAC descriptors in the Host memory with different descriptor elements like Buffers sizes, Buffer addresses programmed appropriately.
  • For the first descriptor, FS(First Descriptor) bit in the first descriptor element should be set to inform the IDMAC that this is the first descriptor. In addition OWN bit should also be set.
  • For Descriptor 2 to Descriptor N-1, OWN bit in the first descriptor element should also be set.
  • For descriptor N(last descriptor in the ring), EOR bit should be set. This informs the IDMAC to load the first descriptor address after finishing the Nth descriptor thus forming a ring.
  • Enable the IDMAC interrupt. Normally IDMAC interrupt occurs when each descriptor finishes. However the individual descriptor interrupt generation can be disabled by setting the  DIC(Disable Interrupt on Completion) bit in the descriptor
  • When the last descriptor interrupt occurs, update all the descriptors in the chain. Do following:
    • Update the Buffer addresses for each descriptor
    • Set the OWN bit for each descriptor(as the IDMAC clears this bit once it executes the descriptor)
    • Write to PLDMND register with any non-zero value to cause the re-fetch of the descriptor.
  • Do this as long as the software needs the descriptor ring to continue.
  • Before the last iteration of the Ring, do the following additional steps(in addition to above mentioned steps) in the last descriptor interrupt :
    • Clear the EOR bit of last descriptor
    • Set the LD (Last Descriptor ) bit of the last descriptor.
  • With EOR cleared and LD set in the last descriptor, the descriptor chain breaks and the IDMAC closes the descriptor operation.