• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)

Q:

How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)?

--------------

A:

Signtool Utility comes along with the CCES package which can be used to sign and encrypt the unsigned loader stream and make it secure.

In order to do this, once we have generated the unsigned bootstream through CCES in binary format following commands can be used to sign and encrypt the bootstream:

Now, how to use SignTool:

  1. To generate a Public/Private key pair

          Signtool genkeypair –algo ecdsa224 –outfile <keypair_file>

   2. To get the public key from the key pair file

          Signtool getkey –key <keypair_file> -type BLKey –outfile <pubkey_file>

   3. To sign a boot image (BLp)

          Signtool sign –type BLp –prikey <keypair_file> -infile <bootstream_file> -outfile <signed_bootstream_file>

   4. To sign and encrypt a boot image (BLx)

          Signtool sign –type BLx –prikey <keypair_file> -enckey <encryption_key_file> -infile <bootstream_file> -outfile <signed_bootstream_file>

          Note: <encryption_key_file> is 128bit encryption key that is used for encryption and decryption

   5. To sign and encrypt a boot image (BLw)

           Signtool sign –type BLx –prikey <keypair_file> -enckey <encryption_key_file> -wrapkey <wrap_key_file> -infile <bootstream_file> -outfile           <signed_bootstream_file>

     Note: <wrap_key_file> holds another 128-bit key which is used to “wrap” the encryption key used to encrypt the boot stream.

Now below command lines shows the same steps used above for a given unsigned bootstream (bootstream.ldr) to add more clearity:

  1. Generate an ECDSA key pair using signtool .

"C:\Analog Devices\CrossCore Embedded Studio 1.1.0\signtool.exe" genkeypair -algo ecdsa224  -outfile keypair.bin

   2. Extract the public key from above generated ECDSA key pair.

            "C:\Analog Devices\CrossCore Embedded Studio 1.1.0\signtool.exe" getkey -key keypair.bin  -type BLKey -outfile pubkey.bin

   3. Now to just sign the unsigned bootstream (bootstream.ldr) use the following command:

"C:\Analog Devices\CrossCore Embedded Studio 1.1.0\signtool.exe" sign -type BLp -prikey keypair.bin -infile bootstream.ldr -outfile blp_signed_bootstream.bin

   4. In order to sign and encrypt the bootstream, two approaches are available:

a. BLx:

"C:\Analog Devices\CrossCore Embedded Studio 1.1.0\signtool.exe" sign -type BLx -prikey keypair.bin -enckey aeskey.bin -infile bootstream.ldr -outfile blx_signed_bootstream.dat

b. BLw:

"C:\Analog Devices\CrossCore Embedded Studio 1.1.0\signtool.exe" sign -type BLw -prikey keypair.bin -enckey aeskey.bin -wrapkey wrapperkey.bin -infile bootstream.ldr -outfile blw_signed_bootstream.dat

Now last step required is to program the corresponding encryption/wrapper key and the public key into the OTP for secure booting.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • How to sign and encrypt a normal bootstream for Secure Boot?
    Sara Collins
    The Normal boot stream can be signed and encrypted using the Signtool utility. The Signtool utility expects the input boot stream/keys to be in binary format and then generates a signed/encrypted image...
  • RE: Secure Boot Loader stream generation
    VineethaThomas
    CCES provides signtool utility to generate secure boot streams in formats Blp, Blx or Blw. A sample command to do the same is given here. The same tool has options to generate the ECDSA key pair and the...
  • Sign and encrypt a normal bootstream: FAQ
    Sara Collins
    Sign and encrypt a normal bootstream: FAQ
 
Related Content
  • How to sign and encrypt a normal bootstream for Secure Boot?
    Sara Collins
    The Normal boot stream can be signed and encrypted using the Signtool utility. The Signtool utility expects the input boot stream/keys to be in binary format and then generates a signed/encrypted image...
  • RE: Secure Boot Loader stream generation
    VineethaThomas
    CCES provides signtool utility to generate secure boot streams in formats Blp, Blx or Blw. A sample command to do the same is given here. The same tool has options to generate the ECDSA key pair and the...
  • Sign and encrypt a normal bootstream: FAQ
    Sara Collins
    Sign and encrypt a normal bootstream: FAQ