Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module

Q:

What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module?

--------------

A:

PKTE module allows the encryption and hashing to be done in parallel. For this two modes are supported. Encrypt-Hash and Hash-Decrypt.


Encrypt-Hash operation mean that the ciphertext obtained from the encryption for a given source input (plaintext) will be used as an input for hashing and then it will produce hash message digest output. So final result will hold the following:

  1. The ciphertext(encrypted output) for a given input
  2. The hash message digest output for a ciphertext generated in step a.


Hash-Decrypt will do the reverse operation of Encrypt-Hash. It will take the ciphertext as input source and will generate the hash message digest output and plaintext(decrypted output) from the ciphertext.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • Hash
    Hash
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: LockBox technology - why use ECC?
    gyi
    Hi Egor, Lockbox is an implementation of ECDSA specified in http://csrc.nist.gov/publications/fips/fips186-3/fips_186-3.pdf 1) It is very difficult for someone to find a matching input that will...
  • LockBox technology - why use ECC?
    Egor
    Hello. What is the benefit from using ECC to encrypt the hash of authentication message? Hacker can always calculate SHA1 of original message by analyzing the contents of external boot-flash (starting...
 
Related Content
  • Hash
    Hash
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: LockBox technology - why use ECC?
    gyi
    Hi Egor, Lockbox is an implementation of ECDSA specified in http://csrc.nist.gov/publications/fips/fips186-3/fips_186-3.pdf 1) It is very difficult for someone to find a matching input that will...
  • LockBox technology - why use ECC?
    Egor
    Hello. What is the benefit from using ECC to encrypt the hash of authentication message? Hacker can always calculate SHA1 of original message by analyzing the contents of external boot-flash (starting...