Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents Performance Enhancements in Blackfin+ core
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

Performance Enhancements in Blackfin+ core

    There are several new features in Blackfin+ core. Some of the Key features which greatly improve performance over existing Blackfin is listed below

  1. Posted system MMR writes

The Blackfin+ core supports posted MMR writes.This feature can be enabled by setting MPWEN bit in SYSCFG register. 

When Posted MMR write is enabled,

  • Core does not wait for a system MMR write to complete before starting another system MMR write.
  • The core does not ensure writes complete in correct order. But system infrastructure will ensure that these writes will complete in the correct order.
  • Core waits for all system MMR writes to complete before issuing a system MMR read. So loads from system MMRs may take longer.


2. Dynamic Branch prediction

    The Blackfin+ core supports dynamic branch prediction. BPEN bit in the SYSCFG register enables the Dynamic Branch prediction. When dynamic Branch prediction is not enabled Static branch prediction is used for predicting branches.


3.16-bit complex multiplication

The Blackfin+ core has new instructions which support 16 bit complex multiplications. The instructions support multiplication of A * B  , A * B’ and A’ * B’ . Where A and B are complex numbers and A’ and B’ are complex conjugate of respective complex numbers. These instructions greatly improve performance of algorithms which involves complex multiplications.


4. Single Cycle *= Multiplication


        *= instruction takes single cycle to complete in Blackfin+ core.

5. 32 bit multiplication

    New 32 * 32 = 64 bit multiplication instructions which support optional saturation and rounding are available.

6. Add with carry and Sub with borrow

New Add with carry and Subtract with borrow with optional saturation instructions are available.


7. Shift instructions

    New Assembly Syntax for Arithmetic right shift with saturation and Arithmetic Left shift are added into new Blackfin+ core

Assembly  Syntax

REG = REG <<< IMM

REG = REG >>> IMM (s)

8.   Not cc to Data register

A new instruction  which enables copying !CC value to Data Register is added.

Assembly Syntax

REG=!CC

This instruction leads to small improvements in compiler generated code as it directly provides a way to copy the inverse of CC value to Data register.


9.Load immediate 32

     In Blackfin+ core ,the immediate 32 bit value can be loaded into Data registers(R register),Pointer registers( P registers, SP,FP), Index  registers(I registers), Modify registers(M register),Length registers(L registers) and Base registers(B registers)


10 .Absolute address Load/Stores

   Load and store from absolute 32 bit address is supported in the core.


11.   Jump/Call to immediate 32

The older Blackfin core allows only 25 bit PC relative address, but in the Blackfin+ core ,Jump and Call can use immediate 32 bit value for PC relative address.


12.    P addressed Load/Store in DAG slot 2

In Parallel instructions, The restriction that if the two 16-bit instructions are memory access instructions only one can use the P-registers as an address register is removed.


13.   TESTSET instruction

In Blackfin+ core, TESTSET instruction can be addressed to any memory byte. These are not cache inhibited access. TESTSET  to cacheable memory region checks cache and update the data in cache.

14.   Scratchpad Memory is same as other L1 data memory

           Blackfin+ core allows DAG and DMA access to scratchpad memory. Hence Scratchpad memory is available to user just as other L1 Data banks.

Tags: bf70x