Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    Latest Webinars

    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
    • Design Smarter with Compact, Low-Power Precision Current Source Signal Chains
    • Power Management Fundamentals II Session 6: Key Layout Considerations for Power
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How many squares, defined...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    Highlighted Blogs

    The New Industrial Robotics Era: Why Innovation Is Compounding

    By Tracey Johnson & Margaret Naughton Imagine a robot stepping out of a safety cage, not to perform a single preprogrammed motion, but to work alongside...

     

    Reimagining Power for AI: Shaping the Future of AI Acceleration: Part 3 of 3

    It’s time to look at the next wave: vertical power delivery and the relentless Analog Devices (ADI) innovation that makes it possible. If you’ve joined...

    Latest Blogs

    • Driving Capacitive Loads Like A Pro: Part 3 of 3
    • Community Spotlight: Meet Akila
    • A Systematic Checklist for RF Transceiver Testing
    • Breaking the Link: Smart Feedback Techniques for Isolated SMPS Regulation: Part 4 of 4
    • Good Marketing Buzz, But How Do I Start?
    Read All Blogs

    ADI Blogs

    • EZ Spotlight
    • The Engineering Mind
  • ContentZone

    Visit ContentZone

    ContentZone

    Technical articles. Blogs. Videos. Your ADI content, all in one place.

    View ContentZone

    Featured Content

    Featured Content Title

    Blurb About Content

    View Content By Industry

    • Aerospace and Defense Systems
    • Automotive Solutions
    • Consumer Technology Solutions
    • Data Center Solutions
    • Energy Solutions
    • Healthcare Solutions
    • Industrial Automation Technology Solutions
    • Instrumentation and Measurement Solutions
    • Intelligent Building Solutions
    • Wireless Communication Solutions

    View Content By Technology

    • A2B Audio Bus
    • ADI OtoSense Predictive Maintenance Solutions
    • Dynamic Speaker Management
    • Gallium Nitride (GaN) Technology
    • Gigabit Multimedia Serial Link (GMSL)
    • Industrial Vision
    • Power Solutions
    • Precision Technology
    • RF
    • Sensor Interfaces
    • SmartMesh
EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents Where can I find power consumption data for BF70x processors?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

Where can I find power consumption data for BF70x processors?

The attached PDF contains a guide to estimate BF70x power. The Excel file can be used as a tool to aid in estimation. Both files should be used in conjunction with the processor's data sheet. Please click "Follow" in order to receive a notification when updates to this FAQ occur.

Attachments:
0654.BF70x_Power_Estimation_Tool_Rev1p0_Aug31-2015.xlsx
3073.BF70x_Power_Estimation_GuideR1_2015-08-31.pdf
Tags: bf703 bf70 power estimation bf707 bf701 bf705 bf706 bf70x bf704 power consumption power bf700 power supply bf702 maximum power consumption Show More