Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
ADSP-BF70x
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
ADSP-BF70x
  • Processors & DSP
  • Blackfin Processors
  • ADSP-BF70x
  • Cancel
ADSP-BF70x
Documents Known Errata Against ADSP-BF70x Blackfin+ Datasheet
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +ADSP BF706 FAQ:
  • +ADSP-BF707: FAQ
  • -ADSP-BF70X: FAQ
    • Different Wake-up Sources on BF70x
    • ADSP-BF70x application cannot boot using Secure Boot
    • CPLB enhancements in Blackfin+ Core
    • FAQ: Different Wake-up Sources on BF70x
    • Digital watch code for RTC
    • Enhancements in Hardware Loop in Blackfin+ core
    • Enhancements in Supervisor Mode in Blackfin+ core
    • HADC maximum bandwidth
    • Highlights of MSI on BF70x
    • How can I initialize DDR memory device connected to BF70x processor ?
    • How do I access the full memory space of the SPI slave?
    • How L2CTL in BF70x is different than BF60x ?
    • How the System Cross Bar (SCB) in BF70x different than in BF60x ?
    • How to configure MSI IDMAC for Dual Buffer Descriptor Ring mode operation
    • FAQ: How to re-enable the Core clock on BF70x after gating it
    • How to send data using SPI READY signal
    • How to take the core out of reset on BF70x
    • How to use the Signtool Utility to encrypt and sign the unsigned bootstream (loader file generated for an application, example:bootstream.ldr)
    • Is INIT Code supported in Secure Boot in ADSP-BF707
    • Monitoring Cache Performance on the ADSP-BF70x
    • Performance Enhancements in Blackfin+ core
    • UART slave boot BF70x with Higher BAUD rate
    • Sample code for HADC on BF70x?
    • What are the salient features of SPI Host Port on BF70x?
    • What is the effect of bus disabling (RDEN bit) on RTC functionality?
    • What is the Encrypt-Hash and Hash-Decrypt mode in PKTE module
    • What is the purpose of the ownership bit when programming the PKTE module for encryption/hashing?
    • What modes of Encryption and Hashing are supported and how do they make an application secure
    • Getting Started with ADSP-BF70x Processors
    • How to re-enable the Core clock on BF70x after gating it
    • Known Errata Against ADSP-BF70x Blackfin+ Datasheet
    • the secret BF70x documentation
    • Where can I find power consumption data for BF70x processors?
    • What are the major differences between DMC module of BF60x and BF70x ?
    • Cache Enhancements in Blackfin+ core
    • Can I pass the output generated from PKA directly to the PKTE module for encryption/decryption
    • Configuring Timer in continuous/single pulse mode
    • ADSP-BF70X BLACKFIN PROCESSOR SUPPORT COMMUNITY
    • DMA error interrupt
    • How to verify that the boot bytes are accurate in all boot modes for the ADSP-BF60x and ADSP-BF70x?

Known Errata Against ADSP-BF70x Blackfin+ Datasheet

We are currently experiencing problems pushing our known documentation errata to the external site, so this Featured Content blurb is going to highlight the known issues:

1> Table 3 (Clock Dividers) on p14 incorrectly indicates that SCLK0 is "Not available on SYS_CLKOUT".  SCLK0 is indeed available as programmed on the part (no divider applied).  The row will be modified to indicate "By 1" in the divider column.

2> In Table 28 (Absolute Maximum Ratings) on p59, the Input Voltage specification is only correct for VDD_EXT(Nominal) = 3.3V.  For VDD_EXT(Nominal) = 1.8V, it is not accurate.  The spec is going to be corrected such that the Rating column is modified from "-0.33 V to +3.60 V" to "-0.33 V to VDD_EXT + 0.2 V", which applies to both 3.3V and 1.8V VDD_EXT(Nominal) ranges. As the upper bound now directly references VDD_EXT, the associated footnote 2 on this table must also be reworded from:

"Applies only when VDD_EXT is within specifications. When VDD_EXT is outside specifications, the range is VDD_EXT +/- 0.2 V."

to

"Applies only when VDD_EXT is within or below specifications."

Tags: adsp-bf703 adsp-bf704 adsp-bf701 errata adsp-bf707 adsp-bf705 adsp-bf702 adsp-bf700 adsp-bf70x datasheet adsp-bf706 Show More
  • Share
  • History
  • More